Please wait
Please wait

À propos WeBeHome

WeBeHome - Well Being Home - wherever you are

Safer and Smarter Home

Security is about much more than just an alarm, a security guard and a decal. It's also about accessibility and control . To know what happens, when it happens. And not only when there is a burglary, but also when the kids come home from school, when the humidity in the basement is too high , when elderly fall or when the heat needs to be turned on in the summer house.

The goal of our work is to use the latest technology to simplify your life so that you can do better things than thinking about "is the basement window really closed?" or "is there risk for mold on attic?" Therefore, we have developed the new generation of active alarm and home appliance service that allows you to easily gain control of the things you want to gain control of in your home, or the cottage - right from your mobile or computer. So you calmly can proceed with the rest of your day.

We offer low or no monthly charges for an online alarm and smart home where you own your the equipment from the start. Instead of expensive monthly fees, call centers manned by guards as many other suppliers provide, we provide a digital portal where you have the option of including a monitor center to get alarm messages if you want and when you want and without subscription.





Customers all over the globe.

WeBeHomes customers are all over the globe

EN-50131-1 certified alarm from WeBeHome

Certified alarm system.

We have a separate base unit for the alarm that communicates on a proprietary protocol with alarm sensors.

The advantages of separating the base unit for the alarm and other types of smart home devices is that the alarm function is more critical. For example, it needs to function even during a power failure, and communication with the sensors should not be disturbed by eg signals from lamps, meters etc. Moreover, it is certified to the European standard for wireless alarm EN 50131-1 grade 2

All sensors and relays that are connected to the base unit can be used in our smart solution, for example, an alarm motion detector can control an Z-wave controlled lighting.


Installation that you can do yourself.

Most people are able to install the alarm system by themselves in a couple of hours. First you connect the Alarm box to the power outlet and a network socket in your router. Then you continue the installation and configuration of accessories using our web portal.

Every installation is unique but follows a few simple guidelines regarding alarm accessories:

  • Mount the base unit in an area where there a wall- and network socket is easily accessed (as well as a phone socket if an alarm through a call is wanted). If the purpose is to use it as an burglar alarm then it is vital that in order to reach it you have to pass a rigged area.
  • Place the magnetic contacts on the front door and set them to be ”active” in home mode in order to create a perimeter protection. Doors that are often used could be given a short delay to reduce risk of false alarms.
  • Place motion detectors in places where potentially unwanted guests have to walk by. Avoid facing the accessories towards windows and heat sources because they may interact with change of light and air streams.
  • The movement detectors are immune to pets (weigh up to 18 kg/40lbs). But, the immunity is heavily affected by pets that are taller or can move around 1m above the floor. Avoid facing the detectors towards stairs if you have pets.

More information is available online on how these and other alarm accessories like smoke detectors, gas alarms, flooding sensors, thermostats etc. should be installed and placed.

Installation of WeBeHome Security System

WeBeHome - Larm och Smarta Hem

The Company

The solution has been in operation on the Swedish security market since 1999. It started off as a wholesales operation with sales to retailers and 2010 it also started with direct sales to end customers. The company was founded as Abell Security Sundsvall AB in 1999. In 2008 the company was divided, the head office moved to Stockholm, and it started to supply services outside Sweden. The name was changed to WeBeHome AB in 2013 to better reflect the offering of both security and smart home. WeBeHome offer a modern, easy to use smart home solution together with an advanced alarm system combined with modern IT-technology.

Some of the areas that we cover are:

  • Burglar alarm
  • A wide range of smart home accessories using Z-Wave
  • Sun shading products like Copenhagen Blinds
  • Camera Surveillance
  • Temperature and humidity monitoring
  • Fire and gas sensors
  • Lighting control
  • Neighborhood watch
  • Door locks

WeBeHome supply the cloud service globally and deliver physical products within the EU. WeBeHome is the owner and operator of the cloud service.


CEO Niclas Gruséus.

Niclas Gruséus took over the company and the role of CEO in 2008 with an aim to reshape the business to take advantage of modern infrastructure and IT technology available today. With over 20 years experience in IT solutions in various industries and a passion to create a solution that makes life easier as homeowners, Niclas has perfect backdrop and momentum. Niclas has education in electricity, telecommunications, economics and later a MBA from Henley Management College.

Niclas Gruseus - CEO for WeBeHome